Hi,
We are currently developing a RFID/NFC reader using the TRF7970A. The transceiver is connected to a STM32F3 using SPI and for now has to support MIFARE classic and, if possible, iCLASS 2k/2. In the future we also want to support NFC, though the exact requirements are not clear yet.
We managed to get the latest RFID reader firmware example working on our hardware and the UID of a MIFARE classic card can be read. We have some questions:
- In some old forum posts a MIFARE development package is referenced that contains source code for reading MIFARE classic cards. Before requesting this package we would like to know if this is the latest version. The reason for asking is that this is quite an old package (2013) and the RFID firmware example itself has also been completely rewritten recently.
- Is there also a development package for reading iCLASS cards with this transceiver? If not, what do you suggest?
- Is there anything we should keep in mind when combining both reading RFID and NFC? As long as this is done sequentially it should work on the same hardware, right?
Best regard,
Martijn