Questions are imbedded in the attached data sheet on page 28, 29, 56 and 60.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Doug,
The questions on 28 & 29 are hard to understand, but I think they are concerning FIFO handling and then I would refer to our example code to understand how we recommend the FIFO to be handled: http://www.ti.com/lit/zip/sloc297
Question on Page 56: Yes, bytes not bits - I will mark that as a typo to fix if we do another DS update
Question on Page 60: It's a threshold, so 9 bytes or more would be accurate as well, but really it's triggered the moment 9 bytes are present in the FIFO and hence the wording. The moment that bit is set, an IRQ will fire, but based on IRQ service time it's not unusual for more than 9 bytes to present by the time the FIFO status is read. Same goes for the 3 bytes on TX threshold which indicates when the FIFO needs to be filled with more data (if applicable).
Can you please ask the customer to not use PDF comments next time? It's not very friendly for me to have to open up a document, scroll through pages, and read comments that are hard to understand because of the formatting of the text...