Other Parts Discussed in Thread: TRF7970A,
Hi,
in past months i have been developing hardware for some temperature and humidity measurements using RFID. Reader part consist of MSP microprocessor and RFID transciever chip TRF7970A, while the sensor part includes some digital sensors that are connected via I2C to RF430FRL152H transponder.
The whole system works great except when i start to increase temperature. The RF430FRL152H chip does not respond when temperature exceeds 60°C. In the datasheet is stated that maximum operating free air temperature is 70°C which would be exceptable for our appplication but 60°C it's a little bit too low. I also read on forum (HERE) that one was able to measure temperature at around 80°C.
My question is what can i do about it? Does the chip shutdown itself when reaches 70°C or it works further on? What can be done if it turns of at 60°C?
Thanks for you reply.
Best Regards
Jan Slapšak