Other Parts Discussed in Thread: CC2541,
Tool/software: Code Composer Studio
Hi TI Folks,
Good day to you.
We are planning to use proprietary mode in 2 Mbps GFSK, the CC2541 is used for sender (TX), the CC2640R2F is used as receiver (RX):
Refer to datasheet, the Data rate and modulation format are as below:
CC2541: 2 Mbps, GFSK, 500-kHz deviation
2 Mbps, GFSK, 320-kHz deviation,
CC2640R2F: 2-Mbps GFSK (Bluetooth 5) – RX --> Frequency error tolerance is -300 kHz ~ 500 kHz
Please advise above plan workable or not?
1. In this communication application, Do both CC2541's 500-kHz and 320-kHz deviation be workable with CC2640R2F?
2. Refer to User's Guide of CC2541 and CC2640R2F: The data package is difference in below:
Please share the more information for this kind of application, and share the example project / code if have.
Best regards
Jiang WeiJi