What exactly is the capability of the PurePath wireless line with regard to 4 channel 24-bit audio? Is it only capable of compressed 24-bit audio or is lossless 24-bit possible? The CC8530 datasheet references uncompressed 24-bit capability, but the user guide does not show a streaming format that supports it. The user guide only offers the SLAC streaming format for 4 channel 24-bit audio, but this is compressed and lossy and results in less than 2 mbps of bandwidth (928 kbps average for 4 channels). However, the CC853X line is capable of 5 mbps of bandwidth so 4 channels of lossless 24-bit audio would easily fit (4.4 megabits). Is this possible and if so, what streaming format should be selected in the configurator to facilitate this? If not, what is the point of 5 mbps capability?