Is there example code that will put the CC2640 into deep sleep and then wake it up on a button press but without the 32kHz crystal? I have seen the normal example of this with the crystal but not without.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there example code that will put the CC2640 into deep sleep and then wake it up on a button press but without the 32kHz crystal? I have seen the normal example of this with the crystal but not without.
The software I used is: tirtos_cc13xx_cc26xx_2_21_00_06 , and pinShutdown example
I modified the ccfg.c to set uo the SCLK_LF source to be RCOSC_LF
//##################################### // Clock settings //##################################### #ifndef SET_CCFG_MODE_CONF_SCLK_LF_OPTION // #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x0 // LF clock derived from High Frequency XOSC // #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x1 // External LF clock // #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x2 // LF XOSC #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION 0x3 // LF RCOSC #endif
which can be found her: C:\ti\tirtos_cc13xx_cc26xx_2_21_00_06\products\cc26xxware_2_24_03_17272\startup_files
The procedure in the application note is only applicable with BLE examples, not for TIDriver examples.
Christin,
Thanks but I'm looking for an example with BLE as per the application note. Is this available or can it be made available to a customer?
Thanks,
Charles