Hi folks.
I have been tasked to investigate the compatibility of the CC1200 as a receiver for transmissions from a CC1101 (configuration details to follow)
The new design needs to include some legacy support for an older product version.
Is it possible to configure the CC1200 to receive MSK packets, sent from a CC1101?
I understand that there are several posts recommending to rather use 2-FSK/GFSK, with modulation index set to 0.5.
This is unfortunately not an option, as there are numerous units in the field, configured to MSK, that need to be supported.
I am aware that with MSK, the CC1101 inverts the sync word, and data to be transmitted.
However, no configuration attempt on my part has been successful.
The CC1101 transmission details are as follows:
433.92MHz
MSK
250kbps
Fixed packet length (20 bytes)
16 bit sync word required
Whitening enabled
(Please advise if I have left out crucial information)
Is it possible to get the CC1200 to receive this type of transmission?
Am I missing something here?
Any advice is greatly appreciated.