Other Parts Discussed in Thread: CC1310
Since the only way to protect the cc1310 processor to be read, is to disable the ti bootloader in the CCFG area
1) After we disable the TI Boot, can we internally read the CCFG area in ram and enable back the ti boot, the flash block and write back the CCFG area?
2) After this we should be able to connect with the TI Boot?
3) Do you have better solution to provide that will allow me to lock my processor to be read and that I can unlock if needed to reprogram it?
3) Are you planning to add a ID code to the back door functionality, with this we could leave the ti boot enabled and access it using the back door and providing the ID code? Ir would be much more useful for manufacturing product with the cc1310 on it?