This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1120 vs CC1101

Other Parts Discussed in Thread: CC1101, CC1120

Hi,

  We have been using the CC1101 so far. Want to move to CC1120 to take advantage of higher sensitivity. Noticed that the sensitivity is given for PER of 1 % (20 bytes  packet length) in CC1101  but it is specified for 1 % BER in the CC1120 data sheet.

Our sensor network runs at 10 kbps (GFSK) or 38.4 kbps (GFSK). Can we get the sensitivity numbers at these two rates (in BER/PER) for the two parts when using the least rx filter bandwidth ? Any other advantages of going from CC1101 to CC1120 ? 

Thx

Ram

  • The relationship between BER and PER can be found here: en.wikipedia.org/.../Bit_error_rate. For CC1120 a PER = 20 % and payload equal to 3 bytes were used. The sensitivity numbers for 38.4 kbps are stated in the CC1101/ CC1120 datasheets

    - CC1120 has better selectivity/ blocking numbers making it more robust in a noisy RF environment.
    - CC1120 sync search is correlator based giving a lot lot lower probability for false syncs than CC1101
    - CC1120 has the ability for RX sniff mode which enables very low Rx current consumption.