Other Parts Discussed in Thread: SIMPLICITI
I have written some code based on the AP as data hub but was seeing random, spontaneous reseting so I went back to the original, unmodified AP as data hub example because I felt like make something was going on with the WDT.
When I tried to compile the example, the message I got back was:
Error[Pa045]: function "__low_level_init" has no prototype C:\Texas Instruments\SimpliciTI-IAR-1.1.1\Components\bsp\boards\EXP461x\bsp_board.c 82
However, I looked and found in C:\Texas Instruments\SimpliciTI-IAR-1.1.1\Components\bsp\mcus\bsp_msp430_defs.h:
/* Initialization call provided in IAR environment before standard C-startup */
#include <intrinsics.h>
#define BSP_EARLY_INIT(void) __intrinsic int __low_level_init(void)
So, while the code that I wrote WOULD compile but would also reset, the example code would NOT compile.
So, I uninstalled SimpliciTI and removed the related folder to be sure. I reinstalled it but got the same error when trying to run the example file.
I then uninstalled IAR and removed the related folders in C:\program files. I reinstalled it but still got the same error.
Google search is turning up NOTHING. Does anyone have any ideas?