Other Parts Discussed in Thread: CC1101, CC110L
Dear experts on TI forum,
I'm trying to use CC1101/CC110L to receive packets of TPMS sensor at 315 MHz and 433.92 MHz.
I'm using two RF1101SE-V3.0 module bought from Amazon and currently I'm able to: transmit packets from 1 module and receive the packet from the other; receive a bunch of packets (unknown source) after I disable address check.
I have been using settings calculated by SmartRF studio.
However, I still cannot receive packet from the TPMS transmitter. The TPMS is using Infineon's SP37 chip and sending packet using 433MHz FSK.
My question is what Sync Word should I use, or should I stay with 0xD3 and 0x91?
What bandwidth, channel spacing and deviation should I use to receive from TPMS?
What else should I configure in the settings?
Your help is greatly appreciated!!
Best regards,
B. Sun