Hi,
I’m having trouble with enabling debug interface with “Forced Mass Erase” function that provides SmratRF Flash Programmer 2.
I’m using CC13xxEM-7XD board on a SmratRF06 Evaluation Board (XDS100v3 debug probe).
Status when using Forced Mass Erase:
>Initiate access to target: XDS-06EB122F1227A.>Failed to read target memory.>Error while reading memory range. Address 0x40091090. >Start flash erase ...>Erase finished successfully.>Reset target ...>Reset of target successfull.Status when uploading a program in to flash:
>Initiate access to target: XDS-06EB122F1227A.>Failed to read target memory.>Error while reading memory range. Address 0x40091090.>Debug interface is locked. Aborting action. Only forced mass erase is possible. >Reset target ...>Reset of target successfull.Is it maybe the flash that is broken?
I also tried the Forced Mass Erase and programming the flash on another same board set and it works. So I assume there is some hardware issues.
Daniel