This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CC430 RF packet handling

Other Parts Discussed in Thread: SIMPLICITI, CC430F5137

Tool/software: Code Composer Studio

Hi

I have enthusiastic project with CC430 chips: two CC430 modules (TE-СС430EV-868), one sending, the other is receiving. Between them is 1 meter of open space. Both with variable length mode, CRC-check and receiver append RSSI and LQI bytes (PKTCTRL1 = 0b101).

Issues:

1. CRC always fail, but data always good;

2. RSSI and LQI bytes, appended to RX packet, do not match with bytes in RSSI and LQI registers;

3. There is 3 bytes appended to my payload on RX side, but must be only 2 (RSSI and LQI);

4. Packet length must be 1 byte bigger than actual payload length dispite the datasheet: "The packet length is defined as the payload data, excluding the length byte and the optional CRC."

Who can give advice on these issues?