Tool/software: TI-RTOS
Hi,
The CC1310 datasheet says that the maximum SPI bitrate is 4Mbps.
I am using the SPI to access a external flash memory, it is working but I need to access it a lot faster.
My product have a display which uses some bitmaps that are stored in the external flash. I am not able to achieve the needed display update frame because I am taking to long to get the bitmaps from the external memory.
My memory can be accessed at 100Mbps, but the CC1310 is capped at 4Mbps.
Is there a way to increase that bitrate?