Dear All,
I modified CONFIG_PHY_ID from APIMAC_STD_US_915_PHY_1 to APIMAC_GENERIC_CHINA_LRM_433_PHY_130.
I have encountered a problem now.
The device with 433Mhz band has to wait for 24 seconds to join with co_processor.
My qeustion is:
1. Is there any difference between 915Mhz & 433Mhz tune to channel function of MAC layer?
It seems that the tune to channel function needs more time to respond the device scan request.
My config and debug message are as below :
AUTO_START: enabled
config.h
#define CONFIG_PHY_ID (APIMAC_GENERIC_CHINA_LRM_433_PHY_130)
features.h
/*! If defined, builds the image with non beacon mode of operation */
#define FEATURE_NON_BEACON_MODE
static void sendScanReq(ApiMac_scantype_t type)
{
System_printf("\n sendScanReq sendScanReq :%d \n",type);
}
ApiMac_status_t ApiMac_mlmeScanReq(ApiMac_mlmeScanReq_t *pData)
{
Board_Led_toggle(board_led_type_LED3);
System_printf("\n ApiMac_mlmeScanReq \n");
}