Part Number: LAUNCHXL-CC1350
Other Parts Discussed in Thread: CC1310, CC1350
Tool/software: Code Composer Studio
hi,
i am working with LAUNCHPAD-CC1350 and i am new in it.
i have launched the primiray examples and now i wrote my own project.
I've combined two examples(rfPacketRx and uartecho with the help of adcbufcontinuous) for getting packets and give theme to pc terminal through UART.
my program just work one time and after that it stop and doesn't work any more.
could anybody help me?
the Sending Launchpad is Working fine and this is my Receiver Side program.
/*
* Copyright (c) 2015-2016, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/***** Includes *****/
#include <stdlib.h>
#include <xdc/std.h>
#include <xdc/cfg/global.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
/* Drivers */
#include <ti/drivers/rf/RF.h>
#include <ti/drivers/PIN.h>
#include <ti/drivers/UART.h>
#include <driverlib/rf_prop_mailbox.h>
/* Board Header files */
#include "Board.h"
#include "RFQueue.h"
#include "smartrf_settings/smartrf_settings.h"
#include <stdlib.h>
/* Pin driver handle */
static PIN_Handle ledPinHandle;
static PIN_State ledPinState;
/*
* Application LED pin configuration table:
* - All LEDs board LEDs are off.
*/
PIN_Config pinTable[] = {
Board_LED1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
Board_LED2 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
PIN_TERMINATE
};
/***** Defines *****/
#define TASK_STACK_SIZE 1024
/* Packet RX Configuration */
#define DATA_ENTRY_HEADER_SIZE 8 /* Constant header size of a Generic Data Entry */
#define MAX_LENGTH 30 /* Max length byte the radio will accept */
#define NUM_DATA_ENTRIES 2 /* NOTE: Only two data entries supported at the moment */
#define NUM_APPENDED_BYTES 2 /* The Data Entries data field will contain:
* 1 Header byte (RF_cmdPropRx.rxConf.bIncludeHdr = 0x1)
* Max 30 payload bytes
* 1 status byte (RF_cmdPropRx.rxConf.bAppendStatus = 0x1) */
/***** Prototypes *****/
static void TaskFunction(UArg arg0, UArg arg1);
/***** Variable declarations *****/
static Task_Params TaskParams;
Task_Struct rxTask; /* not static so you can see in ROV */
static uint8_t TaskStack[TASK_STACK_SIZE];
static RF_Object rfObject;
static RF_Handle rfHandle;
/* Buffer which contains all Data Entries for receiving data.
* Pragmas are needed to make sure this buffer is 4 byte aligned (requirement from the RF Core) */
#if defined(__TI_COMPILER_VERSION__)
#pragma DATA_ALIGN (rxDataEntryBuffer, 4);
static uint8_t rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
MAX_LENGTH,
NUM_APPENDED_BYTES)];
#elif defined(__IAR_SYSTEMS_ICC__)
#pragma data_alignment = 4
static uint8_t rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
MAX_LENGTH,
NUM_APPENDED_BYTES)];
#elif defined(__GNUC__)
static uint8_t rxDataEntryBuffer [RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
MAX_LENGTH, NUM_APPENDED_BYTES)] __attribute__ ((aligned (4)));
#else
#error This compiler is not supported.
#endif
/* Receive dataQueue for RF Core to fill in data */
static dataQueue_t dataQueue;
static rfc_dataEntryGeneral_t* currentDataEntry;
static uint8_t packetLength;
static uint8_t* packetDataPointer;
static uint8_t packet[MAX_LENGTH + NUM_APPENDED_BYTES - 1]; /* The length byte is stored in a separate variable */
uint16_t PAYLOAD_LENGTH=0;
char uartTxBuffer[MAX_LENGTH];
UART_Handle uart;
/***** Function definitions *****/
/*
* This function is called whenever a buffer is full.
* The content of the buffer is then converted into human-readable format and
* sent to the PC via UART.
*
*/
void uartTxPacket_Send(RF_Handle h, RF_CmdHandle ch, RF_EventMask e) {
uint_fast16_t i;
uint_fast16_t uartTxBufferOffset=0;
if (e & RF_EventRxEntryDone)
{
/* Toggle pin to indicate RX */
PIN_setOutputValue(ledPinHandle, Board_LED2,!PIN_getOutputValue(Board_LED2));
/* Get current unhandled data entry */
currentDataEntry = RFQueue_getDataEntry();
/* Handle the packet data, located at ¤tDataEntry->data:
* - Length is the first byte with the current configuration
* - Data starts from the second byte */
packetLength = *(uint8_t*)(¤tDataEntry->data);
packetDataPointer = (uint8_t*)(¤tDataEntry->data + 1);
/* Copy the payload + the status byte to the packet variable */
memcpy(packet, packetDataPointer, (packetLength + 1));
RFQueue_nextEntry();
/*
* Start with a header message and convert each entry in the current buffer
* to a human-readable format
*/
uartTxBufferOffset = System_sprintf(uartTxBuffer,
"\r\nBuffer %u finished:\r\n", PAYLOAD_LENGTH++);
for (i = 0; i < MAX_LENGTH; i++) {
uartTxBufferOffset += System_sprintf(uartTxBuffer + uartTxBufferOffset,
"%u,", packet[i]);
}
uartTxBuffer[uartTxBufferOffset] = '\n';
/* Send out the data via UART */
UART_write(uart, uartTxBuffer, uartTxBufferOffset + 1);
}
PAYLOAD_LENGTH=0;
}
/*
* Callback function to use the UART in callback mode. It does nothing.
*/
void uartCallback(UART_Handle handle, void *buf, size_t count) {
return;
}
void Task_init() {
Task_Params_init(&TaskParams);
TaskParams.stackSize = TASK_STACK_SIZE;
TaskParams.stack = &TaskStack;
//TaskParams.arg0 = (UInt)1000000;
Task_construct(&rxTask, TaskFunction, &TaskParams, NULL);
}
static void TaskFunction(UArg arg0, UArg arg1)
{
UART_Params uartParams;
const char echoPrompt[] = "\fRF Rx :\r\n";
RF_Params rfParams;
RF_Params_init(&rfParams);
/* Create a UART with data processing off. */
UART_Params_init(&uartParams);
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.writeMode = UART_MODE_CALLBACK;
uartParams.writeCallback = uartCallback;
uartParams.baudRate = 115200;
uart = UART_open(Board_UART0, &uartParams);
if (uart == NULL) {
System_abort("Error opening the UART");
}
UART_write(uart, echoPrompt, sizeof(echoPrompt));
if( RFQueue_defineQueue(&dataQueue,
rxDataEntryBuffer,
sizeof(rxDataEntryBuffer),
NUM_DATA_ENTRIES,
MAX_LENGTH + NUM_APPENDED_BYTES))
{
/* Failed to allocate space for all data entries */
while(1);
}
/* Modify CMD_PROP_RX command for application needs */
RF_cmdPropRx.pQueue = &dataQueue; /* Set the Data Entity queue for received data */
RF_cmdPropRx.rxConf.bAutoFlushIgnored = 1; /* Discard ignored packets from Rx queue */
RF_cmdPropRx.rxConf.bAutoFlushCrcErr = 1; /* Discard packets with CRC error from Rx queue */
RF_cmdPropRx.maxPktLen = MAX_LENGTH; /* Implement packet length filtering to avoid PROP_ERROR_RXBUF */
RF_cmdPropRx.pktConf.bRepeatOk = 1;
RF_cmdPropRx.pktConf.bRepeatNok = 1;
/* Request access to the radio */
rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);
/* Set the frequency */
RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);
/* Enter RX mode and stay forever in RX */
RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropRx, RF_PriorityNormal, &uartTxPacket_Send, IRQ_RX_ENTRY_DONE);
while(1);
}
/*
* ======== main ========
*/
int main(void)
{
/* Call board init functions. */
Board_initGeneral();
Board_initUART();
/* Open LED pins */
ledPinHandle = PIN_open(&ledPinState, pinTable);
if(!ledPinHandle)
{
System_abort("Error initializing board LED pins\n");
}
/* Initialize task */
Task_init();
/* Start BIOS */
BIOS_start();
return (0);
}
did anyone know a complete example or project?