Other Parts Discussed in Thread: CC2538, , TEST2, CC-ANTENNA-DK2
Hello all,
I'm working in a custom board using cc2538 for zigbee and cc1200 at 169MHz connected to cc2538 over spi.
The cc1200 has an external PA - 65367_11 Skyworks - up to 27dBm Tx power, no diversity, SMD antenna -2dB Peak Gain.
My problem is that even with Smart RF Studio default settings (Generic 169MHZ, Symbol rate: 1.2kbps, 2-FSK, 12.5 kHz, 10.9 Rx Filter BW) & Tx power at 27dBm,
I cannot get a link greater than 400 meter in Packet tests.
Also the best RSSI I can get without packet loss is around -90dBm.
Using a spectrum analyzer the noise floor in my area is around -100dBm.
On my tests, my devices are 1.5 meter from ground.
Could anyone help me on this?
Thanks in advance,
Spiros