Other Parts Discussed in Thread: CC1310
Tool/software: TI-RTOS
Hi Team,
In our SDK project rfWakeonRadioRx.c, How to change PQT? I would like to make PQT smaller for improving the sensitivity and range.
Best Regards,
Eggsy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI-RTOS
Hi Team,
In our SDK project rfWakeonRadioRx.c, How to change PQT? I would like to make PQT smaller for improving the sensitivity and range.
Best Regards,
Eggsy
Hi TER,
Thank you!
But I have a question.
Let call working without WOR mode A, call working with WOR (numCorr=1) mode B and call working with WOR (numCorr=2) mode C.
I tested their translation distance, I found the translation distance, mode A > mode B > mode C.
I guess the numCorr is bigger , will make it less likely to find preamble in noise, which will also be harder to receive the packet and impact the translation distance.
Do you think so ?
Hi Egsy,
I don't think that you need to change the correlation period. In the WoR RX example, the csEndTime is much shorter (about 650µs) than correlationPeriod (about 960µs) and an evaluation is forced at that time. If the number of correlation tops has not reached corrConfig.numCorrBusy until csEndTime, the correlation result remains "INVALID" and hence, the channel is treated as "INVALID" (csConf.operation is 1, see table 10 here.
If I understand your original post correctly, then you want to make the carrier sense operation less strict. Therefore, you should increase csEndTime. Try to increase it in steps of 100 µs. But this will make it also more likely that the sniff command reports a BUSY channel when there is an interferer. Increasing the sensitivity with this wake-on-radio system architecture has to come at a certain cost, which is always power consumption.