Part Number: CC1350
Other Parts Discussed in Thread: CC1310
I've been doing a bit for reading up and pieced together some information, but there are still a few unknowns for me when it comes to the antenna and RF setup of the CC1350.
- According to this thread, an integrated balun for the device didn't exist as of march 2017 but work was underway on a Sub-Ghz/2.4GHz one. Does it exist yet?
- In terms of antenna, it seems the options are either go the SensorTag route or Launchpad route
- Sensortag: Two single-ended antennas for each frequency, Less complex, but reduced power and sensitivity.
I can't, however, tell which 2.4GHz antenna was used on the Sensortag, though it does look similar to AN043 - Launchpad: Use an RF switch to have both antennas set up differentially. More complex, and likely can't use integrated baluns without experimentation/compensation due to them not being matched to the switch itself.
- Sensortag: Two single-ended antennas for each frequency, Less complex, but reduced power and sensitivity.
- I haven't found any information/designs that outline how to go about using a dual-band antenna, for which there are a few designs in the antenna DK. How would I go about doing this?
In general, I guess I'd like an update on the state of RF possibilities for a dual-band system based on the CC1350. I'm hoping to get a design using it finished in the next week so would like to fully understand my options before then if possible.
Thanks!