Other Parts Discussed in Thread: CC1310, SYSBIOS
Tool/software: Code Composer Studio
Hello!
I followed instructions in rfWsnNodeIntFlashOadClient\Readme.md to build Image A, but project failed to build, because of big size of output .bin file (72k).
It's strange, but then i tried to do the same thing in November - all works fine, since November i got several auto-updates in CCS.
I tried to replace *.c and *.h files in rfWsnNodeIntFlashOadClient with files from my project. Project compiles and works fine, but size of output .bin also rised:
from 45k to 52k with Optimization level = 4
from 54k to 61k with Optimization level = off
+10% of size is to much for me because of small Internal flash size.
1. How can i fix it?
2. What settings i must do in my project (based on Simplelink_cc13x0_sdk_1_50) to implement OnChip OAD? I tried to copy .cmd and .cfg files from rfWsnNodeIntFlashOadClient, but got 15 build errors.
3. In rfWsnNodeIntFlashOadClient Hwi are not disabled while writing/erasing the flash. Is it right?
4. I found a small mistake in Readme.md:
"python /usr/bin/hexmerge.py -o app_v1-all.hex "--overlap=error" app_v1.bin bim_intflash_cc1350lp.hex"
must be
"python /usr/bin/hexmerge.py -o app_v1-all.hex "--overlap=error" app_v1.hex bim_intflash_cc1350lp.hex"
My rfWsnNodeIntFlashOadClient project in attach.