Other Parts Discussed in Thread: CC1350, CC-DEVPACK-DEBUG, MSP-EXP430F5529LP,
Tool/software: Code Composer Studio
Hi All,
I recently got burned by assuming the wifi sensortag development kit was suitable for development (hint, its not). I think the CC1350 SensorTag is, but it has the same cryptic "recommendation" for development to be done on the launchpad. I'm pretty confident that I can in fact deploy custom code on the CC1350 SensorTag (unlike the wifi version), but I wanted to make extra sure that there are no hidden gotchas.
Here's what I want to do:
Periodically read the orientation via the MPU9250 on the sensortag and transmit that to another device (probably a cc1350 launchpad). Then toggle a GPIO on the launchpad, based on the orientation of the sensortag that it received via the wireless link.
This is a pretty straightforward operation, but I want to make sure I order the right pieces and don't get blindsided by something buried in the forums like I did with the wifi sensortag. Can you guys verify that I can do the above with the following pieces:
C1350STKUS
CC-DEVPACK-DEBUG
LAUNCHXL-CC1350US (just one)
(And obviously a computer for the programming part)
Thanks