Hi Ti,
I am having an issue with the Frequency output of the CC1310.
I am using the 915 MHz band.
I have 2 CC1310 Launchpad boards that use the revision B chip and they always seem to work.
In CW mode they put out around 914.997 MHz.
I have some prebuilt modules with CC1310 Revision A chips.
Sometimes they work and sometimes they don't.
When they don't work, I have observed the CW output on a spectrum analyzer to be 914.957.
Do you know why they are putting out a signal 40 kHz lower than the dev boards?
Is it related to the Rev A vs Rev B chips or something else?
I am using the latest SmartRF studio with latest SDKs and the modulation format is selected using SmartRF studio using 50 kbps 2GFSK.
This may be unrelated, but I cannot find the lines to comment out under pOverrides in the SmartRF studio output as mentioned in the below link:
processors.wiki.ti.com/.../CC1310_rev_B_PCN_information
Thanks,
Nick