Other Parts Discussed in Thread: CC1350, CC1310,
Hi,
I have used this examples as below, when I send the data to Launchpad it, but it can't be received.
e2e.ti.com/.../2178563 cc1350 uart&tisearch=Search-EN-Support
I used FT232 to launchpad.
The connector pin:FT232 TXD---Launchpad RXD.
FT232 RXD--Launchpad TXD.
FT232 CTS--Launchpad RTS(IOID_18).
FT232 RTS--Launchpad CTS(IOID_19).
1) TeraTerm config:Baud rate 115200, data 8, parity none, stop 1 ,flow control hardware.
It can't send data to Launchpad.
2)when I used another config:
#define BOARD_IOID_UART_RTS IOID_UNUSED
#define BOARD_IOID_UART_CTS IOID_UNUSED
TeraTerm config:Baud rate 115200, data 8, parity none, stop 1 ,flow control none.
The FT232 can send data to Launchpad, but the Launchpad cannot receive it.
What wrong with my steps?
Thanks,
Best Regards!
Kanta