Part Number: CC1310
Other Parts Discussed in Thread: CC1350
Hello!
I made a new version of my custom board with cc1310 4x4 and it's not working (chip not recognized by CCS, Smart RF...).
My previous board works fine. Changes in new version: 24 MHz crystal moved, 0 Ohm resistors removed, antenna changed.
Voltages on cc1310 pins looks correct:
11 (VDDS) - 3.17V
12 (DCOUPL) - 1.27V
18 (DCDC_SW) - 1.67V
19 (VDDS) - 3.15V
21 (NRESET) - 2.86V
27 (VDDS) - 3.17V
28 (VDDR) - 1.67V
32 (VDDR) - 1.65V
I checked connection between JTAG/RESET pins on cc1310 and debug probe (i used cc1350 LP) - it's ok.
I tried to remove 24 MHz crystal (to force internal RC OSC) - no success, chip still not recognized.
What else can i check?
My gerbers in attach (cc1310 part is on bottom): WiFi_CC1310_BridgeV5.zip