Other Parts Discussed in Thread: UNIFLASH, CC3100, CC3100BOOST, CC3200
I'm trying to flash service pack to CC3100 using Uniflash, but connection itself fails.
Here's log on Uniflash console when GetVersion
[16:41:48] Begin GetVersion operation.
[16:41:48] INFO: > Executing Operation: Connect
[16:41:50] INFO: setting break signal
[16:41:50] INFO: --- please restart the device ---
[16:42:05] ERROR: ---reading ACK signal failed---
[16:42:07] INFO: setting break signal
[16:42:07] INFO: --- please restart the device ---
[16:42:22] ERROR: ---reading ACK signal failed---
[16:42:24] INFO: setting break signal
[16:42:24] INFO: --- please restart the device ---
[16:42:39] ERROR: ---reading ACK signal failed---
[16:42:41] INFO: setting break signal
[16:42:41] INFO: --- please restart the device ---
[16:42:56] ERROR: ---reading ACK signal failed---
[16:42:56] FATAL: --- Can't connect to device !! ---
[16:42:56] FATAL: Error connecting to the device. Please check your COM port settings. Error code: -3
[16:42:56] INFO: > Executing Operation: Disconnect
[16:42:56] Operation GetVersion returned.
I have all installed drivers and set baud rate to 921600 bit per seconds.
Uniflash Version: 3.2.0.00023
OS : Windows Vista.
What should I do next?