Dear friends:
I was trying to program a bin file I did for cc3200 using uniflash. However, even the programming is successful, CC3200 load board can't start from flash after removing SOP2 pin. The program works fine if I use debug mode. The code I had is a modified version from one of the cc3200 examples. There is no html or anything, only .bin file needs to be loaded in. Please let me know if I did anything wrong.