Other Parts Discussed in Thread: CC3200, CC3200SDK, UNIFLASH
Hi, I am compiling and deploying the CC3200 LaunchXL OOB example with TI’s Code Composer Studio (CCS6), but the OOB example doesn’t seem run the same as it did when it was truly “out of the box” where I'd get the dryer, water temp sensor, and sprinkler demos tab. When I run the ‘oob’ example from CCS, it isn’t using files in
“<Installation path>\CC3200SDK\cc3200-sdk\example\out_of_box\html”,
but some other html content that allows basic configuration of device mode and security, etc. Where is it getting these other web config files if not from my project directory?
For background, I did complete steps to format the serial flash (1MB, secure unchecked) and applied the Service Pack Update 0.5.2 using Uniflash, that completed successfully. I have Rev3.2, and chip is XCC3200HZ.
Is there some other step needed to compile and load all the web content files into flash apart from the project deployment with CCS and the SOP-2 jumper? For example, maybe I need to manually load all these files in the html directory one at a time using the "Add file" button in Uniflash? If so, what's the filepath need to be for each of these in the flash filesystem?
I tried Uniflash and using 'oob.bin' for the /sys/mcuimg.bin file, but that didn't change any of the web content files.
Also, as I'm sure we can get this above item sorted, and I'm learning about this TI platform for the first time, is there a tutorial somewhere explaining TI's approach for linking between the web variables, e.g. temperature sensor referenced as “__SL_G_UTP” and whatever TI javascript is fetching them, maybe the com.TI.tokenPoller.js?
Alex