Other Parts Discussed in Thread: CC3200
Hi,
I am studying the application bootloader with cc3200.
I set the bootmgr.cmd:
/* Application uses internal RAM for program and data */
SRAM_CODE (RWX) : origin = 0x20000000, length = 0x9fff
SRAM_DATA (RWX) : origin = 0x2000a000, length = 0x0fff
#define APP_IMG_SRAM_OFFSET 0x2000b000
The mcuimg1.bin is the blinky demo.I set the cc3200v1p32.cmd :
SRAM_CODE (RWX) : origin = 0x2000b000, length = 0x10000
SRAM_DATA (RWX) : origin = 0x2001b000, length = 0x10000
After i download this file(mcuimg.bin : Application_bootloader . mcuimg1.bin : blinky.bin)
It can run well.
But, I want to add some application to dowmload the mcuing1.bin through httpserver before run the bootloader.After i add this application ,when i debug using ccs,it run well(it can download this mcuimg1.bin and run it).But after i write this bin file to sflash,it does not run.
1、I want to ask,is there some differents between debug and download to sflash.
2、where should i set about this project,if i want to add application.
3、I have to use the address 0x20000000-0x20004000?