Hi,
I Format the lauchpad and I have not been able to flash the OOB. I have download the servicepack_1.0.1.5.0.bin and try to follow the instruction under the UniFlash Quick Start Guide web site but I have not been able to get to the point whee OOB boot up from flash. Furthermore, after I Format the Launchpad, it seems that it also errased the MAC address for this board.
Can you tell me the step by step from Format the Lauchpad to the point that I can get theOOB to boot from flash? If posible, please tell it in a step proceedure wth screen capture (or better yet demonstrate it via a video for youtube).
Back to the detail isntruction example, I show my steps which did not get the OOB to boot from flash but I list them so you can help me correct the steps as necessary:
1. Open CCS Uniflash (note: this latest tool does not show version under help->About). Assume I already established the COM connection
2. On the left pane, select the top option CC31xx/CC32xx Flash Setup and Control
On the right pane, select the following buttons:
3. Select "Format" button -> choose 1MB -> wait till format completed
4. Selet Program button -> do I need to do any configuration first?
5. Select "Service Pack Programming" button -> navigate to the directory containsthe latest servicepack_x.bin (servicepack_1.0.1.5.0.bin as of 3/23/16)
6. Select Image Programming -> navigte to directories where oob.bin and out_of_box.ucf are stored. program them one at a time
C:\ti\CC3200SDK_1.1.0\cc3200-sdk\example\out_of_box\ccs\Release\oob.bin
C:\ti\CC3200SDK_1.1.0\cc3200-sdk\example\out_of_box\html\out_of_box.ucf
7. remove the SOP2 jumper, confirm P58 jumper install fo AP mode; reboot
As I said this proceedure did not work. So please correct what I did wrong.
- what do I need to do next?
- How do I find the MAC address for the device and how do I set it up ?
- What do I do with the options uner CC31xx/CC32xx Config Groups?
Thank you for your help,
Sy