Hi,
I wanted to set the CC3200MOD (launch pad) a static IP even though I knew it is a problematic issue.
so, via UniFlash I program what seemed to be OK.
BUT, when I entered the CCS and compiled and run the wlan_station program, the board started to blink its red led and no IP address was shawn on the Tera Terminal.
Evan when I set default values (dynamic IP address etc) to the module, and reset the board, still nothing.
So, what should I do? there's no ipconfig option, there's no cmd option. the module stuck in some state..
and if I'm talking of the subject- why it is that's hard (or better- impossible) to set the CC3200 with static IP?
Thanks