Other Parts Discussed in Thread: CC3200
Hello,
As part of my project I am trying to connect the CC3200 with the Kentec Display using one of the example codes present in the following link:
http://e2e.ti.com/cfs-file.ashx/__key/communityserver-discussions-components-files/968/7711.get_5F00_time_5F00_lcd.zip mentioned in a post by Jitendra Gupta.
Post:
After adjusting the libraries and the linked resources I am still not able to get the LCD working.
Are there any further changes that I have to make in the Software/ Hardware in order to get it running??
Two of the steps that were mentioned:
Steps to configure LCD with LP:
1. ECOs on LCD board to configure it for 4-wire SPI- R2:1, R3:0, R4:1, R5:0, R6:1, R7:0, R8:1, R9:0, R27:0, R29:1, R24:0, R28:1
where- R2:0 [resistor disconnected], R2:1 [resistor connected]
2. PIN match table with CC3200 LP
I am not able to understand what is meant exactly by the 1st step as well
Regards
Thanks