Part Number: CC3100MODBOOST
Other Parts Discussed in Thread: CC3100, CC3200, CC3100SDK
Hi,
I use a host MCU connected to cc3100modboost via spi.
The MCU get the data from UART sensor and post it via http to the server.
i use CC3100SDK_1.2.0 and CC3100_CC3200_ServicePack_1.0.1.6-2.7.0.0
i have a strange behavior.
after few minutes of a good trannsmition the code of the MCU stuck in function :
static _SlReturnVal_t _SlDrvRxHdrRead(_u8 *pBuf, _u8 *pAlignSize)
while (SearchSync && TimeoutState)
{
...
}
Any idea?