This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC3220S-LAUNCHXL: Cannot Connect to the Board after Updating to Uniflash 4.2.0.1435

Part Number: CC3220S-LAUNCHXL
Other Parts Discussed in Thread: UNIFLASH

Tool/software: Code Composer Studio

Hi,

I didn't have any problems connecting to my board (CC3220S-LAUNCHXL) using Uniflash on my Ubuntu machine till this morning when I updated my Uniflash to 4.2.0.1435 version. Since I get "Operation Failed: Timeout reading data" error when I try to connect to the board in Uniflash. I uninstalled Uniflash completely and installed the old version but the problem didn't go away.

UPDATE 1: This is the console output when I execute ./dslite.sh --mode cc3220 device info in a terminal:

INFO:root:FTDI not detected, trying XDS
INFO:slbootloader.slbootloader:Connecting to device
INFO:slbootloader.slbootloader:Power off
INFO:slbootloader.slbootloader:Set break signal
INFO:slbootloader.slbootloader:Power on
Traceback (most recent call last):
File "<string>", line 2611, in <module>
File "<string>", line 2607, in main
File "<string>", line 2587, in cmdline
File "<string>", line 2382, in command_device_info
File "<string>", line 587, in connect_device
File "/home/user/Downloads/sl_image_creator/slbootloader/slbootloader.py", line 392, in connect_with_reset
File "/home/user/Downloads/sl_image_creator/slbootloader/slbootloader.py", line 276, in _expect_ack
File "/home/user/Downloads/sl_image_creator/slbootloader/slbootloader.py", line 307, in _read_data
slbootloader.slbootloader.BootLoaderError: Timeout reading data
SLImageCreator returned -1

Can anybody help me?

Regards,

Aydin