Other Parts Discussed in Thread: UNIFLASH, , CC31XXEMUBOOST
Hi,
I need to use the Radio Tool in order to test the performance of my design and improve the antenna matching. My design is based on the BoosterPack, I'm using UART to connect (RX, TX and nHIB).
Uniflash connects successfully and after flashing the Service Pack 3.7 (sp_3.7.0.1_2.0.0.0_2.2.0.6) I manage to connect to the AP and the webserver works nice.
I'm using the Radio Tool 1.0.2, and so far the app doesn't connect to it. I've tried tying RTS and CTS also but no change.
Am I missing some connection or I need to flash a different version of the Service Pack? The RadioTool doc (SWRU471) point me to the wiki () but I get a permission error (
You do not have permission to read this page, for the following reason: