Other Parts Discussed in Thread: WL1271
Hello all,
I am trying to setup a wifi module (wl12xx) in MMC2 (mmc0, MMC1, MMC2) in AM335x, but I'm always getting the same message:
[ 15.480617] mmc2: queuing unknown CIS tuple 0x0f (0 bytes)
[ 15.487081] mmc2: queuing unknown CIS tuple 0x03 (0 bytes)
[ 15.589693] mmc2: queuing unknown CIS tuple 0x01 (0 bytes)
[ 15.595537] mmc2: queuing unknown CIS tuple 0x10 (0 bytes)
[ 15.601843] mmc2: queuing unknown CIS tuple 0x04 (0 bytes)
[ 15.610737] mmc2: queuing unknown CIS tuple 0x3f (0 bytes)
[ 15.703955] mmc2: queuing unknown CIS tuple 0x04 (0 bytes)
[ 15.710504] mmc2: queuing unknown CIS tuple 0x01 (0 bytes)
[ 15.717756] mmc2: queuing unknown CIS tuple 0x3f (0 bytes)
[ 15.811368] mmc2: queuing unknown CIS tuple 0x04 (0 bytes)
[ 18.602396] mmc2: error -22 whilst initialising SDIO card
I checked all the signs as suggested in:
processors.wiki.ti.com/.../WL18xx_Platform_Integration_Guide
My device tree:
mmc3_pins: pinmux_mmc3_pins {
pinctrl-single,pins = <
0x74 (PIN_INPUT_PULLUP | MUX_MODE7) /* gpmc_wpn.gpio0_31 */
0x44 (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_a1.mmc2_dat0 */
0x48 (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_a2.mmc2_dat1 */
0x4C (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_a3.mmc2_dat2 */
0x78 (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_ben1.mmc2_dat3 */
0x88 (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_csn3.mmc2_cmd */
0x8C (PIN_INPUT_PULLUP | MUX_MODE3) /* gpmc_clk.mmc2_clk */
>;
};
wl12xx_gpio: pinmux_wl12xx_gpio {
pinctrl-single,pins = <
0x7c (PIN_OUTPUT_PULLUP | MUX_MODE7) /* gpmc_csn0.gpio1_29 */
>;
};
wl12xx_vmmc: fixedregulator@2 {
pinctrl-names = "default";
pinctrl-0 = <&wl12xx_gpio>;
compatible = "regulator-fixed";
regulator-name = "vwl1271";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
gpio = <&gpio1 29 0>;
startup-delay-us = <70000>;
enable-active-high;
};
&edma {
ti,edma-xbar-event-map = /bits/ 16 <1 12
2 13>;
};
&mmc3 {
/*these are on the crossbar and are outlined in the
xbar-event-map element */
dmas = <&edma 12
&edma 13>;
dma-names = "tx", "rx";
status = "okay";
vmmc-supply = <&wl12xx_vmmc>;
bus-width = <4>;
pinctrl-names = "default";
pinctrl-0 = <&mmc3_pins>;
ti,dual-volt;
ti,non-removable;
cap-power-off-card;
keep-power-in-suspend;
};
Any error in my configuration?
This error may be hardware?
I'm using the kernel by Robert Nelson. eewiki.net/.../BeagleBone+Black
Thanks
Fabio