Other Parts Discussed in Thread: WL1835MOD
We have found below data from wpa_supplicant "README-P2P"
=================================================================
p2p_group_add [persistent|persistent=<network id>] [freq=<freq in MHz>]
[ht40] [vht]
Set up a P2P group owner manually (i.e., without group owner
negotiation with a specific peer). This is also known as autonomous
GO. Optional persistent=<network id> can be used to specify restart of
a persistent group. Optional freq=<freq in MHz> can be used to force
the GO to be started on a specific frequency. Special freq=2 or freq=5
options can be used to request the best 2.4 GHz or 5 GHz band channel
to be selected automatically.
=================================================================
In case of setting Freq =2 (also using 2.4GHz ) as above , if GO makes group, there are searching and setting optimal Frequency automatically? Is this also working at wl1835MOD?
Or as above, is there extra function, which is searching and setting optimal Frequency automatically when GO makes Group at WIFI-DIRECT P2P?