Other Parts Discussed in Thread: WL1837, WL1837MOD
Hi,
I am planning to use WL1837MOD in single Antenna configuration. In the reference design of WL1837 both chip antennae have been used and they are more than 60mm away from each other. If I only have to use single antenna how far would it be placed from the module and what would be the characteristics of the RF trace to the antenna feed point. The device in which this module will be used has a form factor of 55mm x 35mm. Due to the form factor constraint i will need to modify the pcb layout I haven't found any useful information regarding this so any help would be really appreciated.
Thanks.
Hur