Other Parts Discussed in Thread: WL1835MOD
Team,
There are some power consumption information at different places in the "WL1835MOD datasheet - SWRS152L" and “WL18xx Module HW intergartion UG - SWRU437”.
I am trying to find out how all the figures relate to each other in the WLAN use case.
For VBAT we have:
a) "Maximum power dissipation: 2.8 W" in section 5.4 of SWRS152L:
http://www.ti.com/product/WL1835MOD/datasheet/specifications#SWRA1702340
b) For calibration in table 6-1 of SWRS152L we have 3.6V x 850mA (which would be appr. 3.1W) on VBAT:
http://www.ti.com/product/WL1835MOD/datasheet/detailed_description#SWRS1526797
I understand note 2 as if the 30% are already included in the 850mA figures.
c) SWRU437 table-6 page 12 gives maximum current values:
3.6V at 1A which makes 3.6W.
Q1: I think that b) superseed all the other information. The VBAT power supply must meet this power specification. Correct?
Or should 30% margin be added to the 850mA and c) would be the specification to meet?
Q2: At what VBAT voltage does this current value correspond to?
Do we have some information on what max current is at different VBAT? or should we assume 850mA max in all cases?
Q3: To what scenario does a) correspond to (VBAT voltage/current and VIO voltage/current)?
- For VIO:
a) SWRU437 table-6 page 12 gives:
1.8V at 200mA
b) I did not find any max current for VIO.
Q1: Assuming that a) gives the max current for VIO:
on what use case is this maximum reached?
I guess that the SDIO activity the highest contributor to the VIO power. So the VIO power consumption depends on how much data are sent/received. Correct?
Any additional info available on the VIO current pattern?
Q2: what would be the VIO current consumption corresponding to the calibration phase? Should we assume 200mA?
Thanks in advance,
A.