Hi,
I have noticed that Android device using WiLink chipset is terminating once and then Block Ack Session for downlink data stream (AP -> WiLink8 device) by transmitting a DELBA with initiator = recipient. What could be the reason that WiLink8 is terminating reception of aggregated frames? Could it be that re-ordering buffer has run full? Would that be a hint that something is not running smoothly on host side of the Android device using WiLink8 Note: Android device has told in ADDBA Response to AP that buffer size is 32 (see packet 13264 of attached airtrace)
Btw, why is transmitting WL8 DELBA a second time (see below) although first DELBA has been alreadyWL18 acked by AP?