Tool/software: Linux
Hi,
I am using the WL1837MOD with the WL18XXMODCOMSDMMC adapter (100 pin to sdcard).
I am trying to make it work on my laptop (not a custom board). This is a common x64 Dell laptop with Ubuntu Xenial.
Here is the dmesg output when I plug it in:
rtsx_pci_sdmmc rtsx_pci_sdmmc.0: card claims to support voltages below defined range mmc0: new high speed SDIO card at address 0001 wl1271_sdio: probe of mmc0:0001:2 failed with error -61
When I dig in the Linux driver code, the issue is the call to wlcore_probe_of (wlcore/sdio.c).
Two cases:
- Default kernel: CONFIG_OF