This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5100A: Can PCM5100A support half rate BCK of 22.05k, 24k

Part Number: PCM5100A

Can PCM5100A support half rate BCK of 22.05k, 24k sample colck with BCK use internal PLL.

I see the part support double clock, but no half clcok support information with hardware mode, thanks

  • Hi,Lanjie,

    The PCM5100A is not intended to operate at "half clock" rates. Altough the device might work with 22.05KHz or 24KHz sample rates, we can only guarantee the correct performance of the device when the sample rates described in System Clock Functions section are used.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer