Other Parts Discussed in Thread: WL1837
Tool/software: Linux
Linux 4.1.15
R8.6_SP1
wlcore: PHY firmware version: Rev 8.2.0.0.233
wlcore: firmware booted (Rev 8.9.0.1.55)
Hello,
We are going through the certification process right now and have received communication about the inability to get the WL1837 to transmit with 40MHz bandwidth when connected to an AP configured for 11n HT40_ch62, ch102. WL1837 successfully connects and transmits, but the the signal bandwidth is only 20MHz.
Is it possible to get the WL1837 to transmit over 5GHz 11n HT40? If so, how to do so and any pitfalls that could occur when attempting to connect with this configuration? I've requested the lab to provide their procedure to connect to AP in order to further assist this issue.
Thanks,
Brandon