Part Number: WL1835MOD
Hi,
I am using WL1835MOD along with the chip antenna used in the EVM board.
But I have to keep the chip antenna on a different board than the board on which the WL1835MOD is kept. I am using a u.FL to u.FL cable to connect both of them.
The datasheet recoomends a 1dB track attenuation to re-use regulatory certifications done. If I follow the same layout as in the EVM till the u.FL connector and use a cable to connect to the antenna on the other board. Can I re-use the certification ? Considering that total length / attenuation will be higher than what is in EVM.
Thanks,
Ganesh