Tool/software: Linux
Hi,
thank to your tuto :
WL18xx TI Bluetooth Stack AUDM Demo App
I managed to connect my android phone with A2DP.
I used
gst-launch-1.0 -v --gst-debug-level=2 ss1a2dpsrc deccaps=sbcdeccaps ! ss1rtpsbcdepay ! capsfilter name=sbcdeccaps ! ss1sbcdec ! alsasink device="hw:0,0"
It was OK.
The things is to upgrade sound quality with mp3 codec.
I made sure the plugin works by listening to a local mp3 file.
I re-compiled SS1BTPM with BTPS_CONFIGURATION_AUD_SUPPORT_MP3 1
I transfered SS1BTPM and libgstss1bluetooth.so, and I restarted my board.
I inspired from the command line with the SBC codec :
gst-launch-1.0 -v --gst-debug-level=2 ss1a2dpsrc deccaps=mp3deccaps ! ss1rtplatmdepay checkmuxfragments=false ! capsfilter name=mp3deccaps ! mad ! alsasink device="hw:0,0"
but unfortunately my gst pipeline didn't work
gst_parse_perform_link: could not link capsfilter0 to mad0
My question is : can I use mad codec to decode MP3 stream ?
Best regards,
Thomas