Tool/software: Linux
Hi,
I am working on wl18xx module. I have compat_wl18xx-1.0 sdk from which i can generate .ko modules. I need to updated compat-wl18xx-1.0 sdk so that i can compile new modules.
Please help soon.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hi,
I am working on wl18xx module. I have compat_wl18xx-1.0 sdk from which i can generate .ko modules. I need to updated compat-wl18xx-1.0 sdk so that i can compile new modules.
Please help soon.
There is no easy path here.
What is the reason you are upgrading you software at this point? What are you using today?
In practice, if you intend to update your software, you have to move to a newer release (R8.7_SP3) in case you also need to have a solution for WPA2 crack.
You can't upgrade the firmware (wl18xx-fw-4.bin) only without moving to newer drivers as the APIs have changed between the kernel (driver modules) and the firmware.
You would have to update your drivers modules, firmware, wl18xx-conf.bin, wpa_supplicant newer one.
Best Regards,
Eyal
Hi Eyal,
Our customer send us the channels on which AP is set.These are the channels:
36,40,44,48,56,60,64,100,108,112,128,136,140
and I have check the frequencies on above channels ,these frequencies are present in GB and US both regions.SO it should work in London also.But we are not able to understand why it does not work.
Note they are using Ruckus APs.
Hi,
There is nothing specific about these channels.
We are not familiar with this specific brand of AP, but I suggest you ask them to try another AP using the same channel that is not working for them now and see if the issue is specific to it.
It could be an issue with the AP itself, its firmware version or many other factors.
I am afraid that without seeing a wifi air sniffer log there is not much you can figure out from this description.
Best Regards,
Eyal