This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/WL1835MOD: R8.7_SP2 driver for kernel 3.0.35 using build script

Part Number: WL1835MOD

Tool/software: Linux

Hi,

Currently we are using R8.6_SP1 driver. We need to upgrade it to R8.7_SP2 driver/firmware for our device as it needs to pass ETSI RED.

The following link says R8.7_SP2 is needed to pass ETSI RED.

e2e.ti.com/.../2260615

Our kernel version is 3.0.35.

My question is that will the R8.7_SP2 supports both FCC and ETSI compliance or we need to have seperate versions for them