Hi all,
We are experiencing 'link abortion' on Bluetooth-RFCOMM links ( that are active for a longer time).
We see this behavior only when using WL18xxMOD based chipsets ( when using other types/brands of Bluetooth devices , this link-aborting is not occuring).
Those links abortions have been experienced in TI-WL18xx , Service Pak 3.9 {wl18xx_bt_sp_v3.9} and 4.2 {wl18xx_bt_sp_v4.2}
When debugging into the Linux-BlueZ kernel the first 'trigger' when such an abortion occurs is seen at "l2cap_disconn_cfm - hcon ee51ec00 reason 8" this error '8' is then translated to error 110 ( timeout) for the applications. { as said before, we do not see these 'link abortions' on other ( none Ti) based chip-sets }
Any hints on how to avoid these 'link' abortions ?
Best Regards,
Noel
PS: HCI-DUMP, TI-logger-tool and SERIAL-logged (between host and WL18xx module) .. logs have been included in attached-zip file.,