Tool/software: Linux
Hello,
I want to use the HFP profile on my custom board (imx6 - wl1837 - BluetopiaPM)
The A2DP profile is already working. I use a gstreamer pipeline with TI pluging as source (ss1a2dpsrc ...).
I'm using BT_HCI to play my A2DP stream.
On my baord, BT_AUD_IN, BT_AUD_OUT and BT_AUD_FSYNC pins are not connected.
According to the HFRM_AG sample (in the LinuxHFRM_AG.c), the gstreamer pipeline uses the WILINK8BT sound card.
I don’t see WILINK8BT in the aplay list command.
1st question: does WILINK8BT use BT_AUD_IN/OUT, BT_AUD_FSYNC pins ?
2nd question: can I use BT_HCI (as for the a2dp) to receive and send HFP streams ?
SIncerely
Thomas.