Other Parts Discussed in Thread: CC2530, Z-STACK
Hi everyone,I am using CC2530 but I don't how to config Coordinator,Router and EndDevice for it.
I have read ZStack-CC2530-2.4.0-1.4.0 but I don't see file config.
Can you help me!
Thank!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
To understand how Zigbee devices are configured as Coordinator, Router, and end device with CC2530-SoC solution I will recommend you to use example applications (Sample/generic/serial) from TI included with Z-Stack-2.4.0-1.4.0 install. Z-stack looks for zgDeviceLogicalType variable value to determine the logical type of the device during start-up which needs to be initilized properly. Also, read section 3.1.2 of Z-stack API document (SWRA195) for how device starts in the network.
Hope this helps.
Regards,
Suyash Jain
thank Suyash Jain. I have seen how config.
I am using IAR Embedded Workbench evaluation version v7.60.
I have some questions :
When I opend project : C:\Texas Instruments\ZStack-CC2530-2.4.0-1.4.0\Projects\zstack\Samples\GenericApp\CC2530DB and I want to creat file HEX as below:
but when done it created file GenericApp.hex has capacity ~ 2,5Mb therefor I can use Flash Programmer 1.10.2 to programe on SmartRF05EB through CC Debuger.
Help me config Linker in picture?
and I want to test tranfer radio between 2 SmartRF05EB then what project in ...ZStack-CC2530-2.4.0-1.4.0\Projects\zstack I can see it? and how created file HEX to programe on SmartRF05EB.What software help me can see frame tranfer?
I am newbie Zigbee therfore can you help me.
Thankyou!
Hello LongLD,
To understand how to generate hex file using IAR-8051 compiler please see the link: http://e2e.ti.com/support/low_power_rf/w/design_notes/how-to-configure-the-iar-ew-8051-to-generate-a-hex-file-for-cc2530-using-z-stack-plus-link-for-cc2430-cc2431.aspx
Hope this helps
Regards,
Suyash Jain