1. How can i get the mac address of the CC2538. In which address MAC Address is stored.
2. If i want to use front end(CC2592), only HAL_PA_LNA compile flag is enough or any thing i need to configure.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. If i am not using Zstack, then how can i get it. I have used CC2541 to get a mac ID from particular address. I want to know that address. So that i can read with out the help of Zstack.
2) I started to use CC2538 Development board. I started with UART. i used HAL driver of Zstack Home .1.21. I noticed that, if i used HAL_UART_PORT0, it is configuring PA0 and PA1 as UART Pins and if use HAL_UART_PORT1, then also it is configuring same port pins. I don't know, where these is configured. I came to know PA0 and PA1 used, by reviewing the schematic of smartRf 06 Board(Correct me, if i am wrong with Port Pins). So, how can i change Port Pins to configure as UART Port.
I have one more question. In custom board, PN and LNA Pin of CC2592 is connected to PD1 and PD2. Then how can i use those pin. I think if i Enable that flag which you have mentioned in earlier post, it will not work for me. Then where i have to change those Port Pins also. Can you answer these 3 question.
Another way to get the mac address:
uint32 macAddrHi = *((uint32*)0x00280028);
uint32 macAddrLo = *((uint32*)0x0028002c);
Put above two together, you get the mac address. Run it before the os tasks start.